Expand a row in the Data Type Editor
Expand a row in the Data Type Editor to display the sub-member name and description.
Expand a row in the Data Type Editor:
- To expand a member row choose one:
- Select
in the row to display the sub-member name and description.
- Right-click the row to expand and selectExpand Member(s).
- To collapse a member row choose one:
- Select
in the row to collapse.
- Right-click the row to collapse and selectCollapse Member(s).TIP:SelectEdit > Expand MemberandEdit > Collapse Memberor pressALT+UPandALT+DOWNto expand and collapse a member row.
TIP:
The
Edit > Expand All Members
and Edit > Collapse All Members
menu commands expand and collapse all members of the data type whose data type is a structure. Note that only the top-level members are expanded and collapsed.Provide Feedback