Embedded - text for Use only the selected Security Authority

  1. (optional) Select Use only the selected Security Authority for authentication and authorization to associate this project with a specific Security Authority. When this check box is selected, users interacting with this project must be authenticated and authorized by the same Security Authority that was used to secure the project. Otherwise, unauthenticated users must rely on Guest User permissions.
    TIP:
    Guest User permissions are cached within the project. The
    Logix Designer
    application uses Guest User permissions when the project is opened but not connected to the
    FactoryTalk
    Security Authority that secures the project. By default, all Guest User permissions are denied. Guest User permissions are configured in the
    FactoryTalk Administration Console
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal