Member Selector window
The
Member Selector
window gives quick access to all decorative elements available as replacements. All parameters and functions added to the current library object, including parameters and functions added to the library objects higher in the library object hierarchy, display in the window. Saved functions and predefined parameters also display.The decorative elements are organized in tabs, with the same features as the tabs in the decorator panel.
New parameters and functions can be added to the project directly from the tabs in the
Member Selector
.Provide Feedback