Copy a substitution

A substitution can be copied to a different library object.
To copy a substitution to a different library object
  1. In the decorator panel, click the
    Substitutions
    tab.
  2. Right-click the substitution, then select
    Copy
    .
  3. Open the library object in which to add the substitution.
  4. Right-click the name of the group in the
    Substitutions
    tab, then select
    Paste
    .
    The substitution is added to the library object.
    TIP:
    The substitution will only take effect in the new location if the text string to be replaced and all decorative elements used in the substitution are contained in the library object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal