Change the order of execution

Substitutions applied at one level of the library object hierarchy extend to all objects at lower levels of the hierarchy, and to all elements that are contained within the library objects. Substitutions applied at a higher level in the hierarchy take precedence over substitutions applied directly to the library object.
To change the order of execution for a substitution
  1. In the decorator pane, click the
    Substitutions
    tab.
  2. Click the substitution, either:
    • On the
      Substitutions
      toolbar, click
      Move Up
      or
      Move Down
      .
    • Right-click the substitution, then select
      Move Up
      or
      Move Down
      .
      TIP:
      Substitutions can also be alphabetically sorted by column content. Click the column name to toggle between ascending and descending sort order.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal