Select Library
Use the
Select Library
window to define the parameters of the linked library. After the library is selected, the parameter will appear in the Parameters browser
window.The table describes the fields in the
Select Library
window.Name | Field Type | Description |
|---|---|---|
Filter | Text Entry | Apply a filter to find the desired selected library object. |
Connect to Database | Button | Connect to a different database to access additional libraries. |
Server ***** | List | Displays selected library objects from other databases or locations. Click to select a library object. |
Provide Feedback