Extended Properties
How do I open Extended Properties?
- InLibrary Objects, select a parameter or tag.
- In the decorator panel, selectTags, then select a tag from the list.
- Select or expandExtended Properties.
Use
Extended Properties
to view, edit, or parameterize the extended properties of a tag.Pass-through values, such as extended properties inherited from other objects, cannot be parameterized in
Library Designer
. Pass-through values are not displayed in Extended Properties
.Pass-through values that are overridden in
Studio 5000 Logix Designer
can be parameterized. Overridden pass-through values are displayed in Extended Properties
.Provide Feedback