Exclude inherited substitutions

Substitutions can be inherited by an element from the containing library object, or from a library object higher in the library object hierarchy (base library). Remove inherited substitutions that are not applicable to an application.
Library object elements supported:
  • Tags
  • Tasks
  • Programs
  • Routines
  • Ladder logic diagram elements
  • Function block diagram elements
  • Sequential function chart elements
  • Structured text chart elements
  • Motion groups
  • Add-On Instructions
  • Data types
  • Modules
To exclude inherited substitutions
  1. In the
    Library Objects
    pane, select a supported library object element. The decorator panel displays the element attributes on the top half of the pane and the element parameters on the bottom half.
  2. In the element attributes section of the decorator panel, select either:
    • Exclude Library Substitutions
      : Remove substitutions that have been inherited from the library object. Reverts to the original value for the element.
    • Exclude Base Library Substitutions
      : Remove substitutions inherited from the base library object for the current library object.
      TIP:
      • If substitutions have also been added to the library object, the field switches to the library object substitution.
      • If no substitutions have been added to the library object, the field reverts to the original value for the element.
  3. Select
    Apply
    , then
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal