Activate a new element

When modifications are made in
Studio 5000 Logix Designer
to an element that has been added to a library object in
Library Designer
, the element must be updated in
Library Designer
to include the modifications. New elements will appear in the parameters section of the decoration pane for the element, but they must be activated so that they are recognized by the
Library Designer
.
This requirement applies to these items:
  • Function block diagrams
  • Sequential function charts
    TIP:
    The connection wires that have a gray color must be activated.
To activate a new element
  • Right-click the connection wire, then select
    Add
    . The wire color on the display changes from gray to black.
    IMPORTANT:
    Default substitutions are inherited automatically. Overrides to the default substitution, and all other decoration, must be applied manually to new elements of an existing library object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal