Interface Member window

How do I open the Interface Member window?
  1. In the decorator pane, click the
    Interfaces
    tab.
  2. In the
    Interface Members
    section, either:
    • Click the interface member, then on the
      Interface Members
      toolbar, click
      Edit
      Edit.
    • Right-click the interface member and then click
      Edit
      .
    • Double-click the interface member.
Use the
Interface Member
window to edit the properties of an interface member. Changes that are made apply to other libraries that use the same interface.
Property
Description
Name
The name of the interface member.
Data Type
The data type of the interface member. This field is read-only.
Value
The value of the interface member. This value can be directly entered or generated by an expression. Click the value and then click the ellipsis (...) button to open the Expression Builder window.
Description
A description of the interface member.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal