Delete or edit interfaces
Delete or edit interfaces as needed.
To delete or edit interfaces
- Select the interface to change.
- To delete an interface, on theInterfacestoolbar, click theDeletebutton or right-click the interface and selectDelete.
- To edit an Interface, on theInterfacestoolbar, click theEditbutton. TheEdit Interfacewindow opens. Change the field values where applicable. TheRevisionfield must be updated.
- (optional) To import additionalInterface Members, select the down arrow.TheSelect Library Interfacewindow opens.
- Connect to a new database by clicking theConnect to Databasebutton.
- Select the file to import.
- SelectOKwhen the desired files are added.
- ClickOK.
Provide Feedback