Add interface members

Add interface members as necessary.
To add interface members
  1. To add interface members, select an interface, either:
    1. Click the
      Add new member
      button located next to
      Interface Members
      .
    2. Right-click the first field and select
      Add New
      .
  2. The
    Tags
    window opens.
  3. Select the tag that will be added and click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal