Add an interface

There are two types of interfaces, input and output. Add an interface as needed.
To add an interface
  1. Select the
    Interfaces
    tab.
  2. In the
    Interfaces
    tab, select
    Add New
    . The Add New Interface window opens.
  3. In
    Name
    , type a name for the interface.
  4. In
    Usage
    , select either:
    • Output
      1. On the
        Interface Members
        toolbar, click
        Add member
        Add member. The
        Tags
        window opens.
      2. Choose a task, program, routine or tag to add as an interface member.
      3. Click
        OK
        to return to the
        Add New Interface
        window.
    • Input
      1. On the
        Interface Members
        toolbar, click
        Import members
        Import members. The
        Select Library Interface
        window opens.
      2. Select a library with a configured output interface. Libraries that have available output interfaces are displayed on the right side of the
        Select Library Interface
        window.
      3. Select available interface members from the
        Interface Members
        grid in the lower right pane.
      4. Click
        OK
        to return to the
        Add New Interface
        window.
  5. In
    Interface Description
    , type a caption to describe the interface.
  6. (for an Input interface) In
    Keying
    , select either:
    • ExactMatch
      . The keys defined for the interface and its members in the project must match the ones defined on the target system for the input to be consumed. The interface and its members can’t be set manually.
    • Disabled
      . Keying attributes are not evaluated when determining whether to consume data from the interface. Member references can be selected manually, however only members with the same data type can be selected.
  7. In
    Key Id
    , enter an identifier that allows for automatic linking of interface members. For automatic linking to occur the KeyId of the input interface must match the KeyId of the output interface.
  8. In
    Revision
    , enter the revision number of the interface link.
  9. In
    Link Name
    , type the name of the library associated with this interface.
  10. Click
    OK
    . The
    OK
    button is not available until the fields are populated.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal