Use a previously created function

Use the
Import
button to reuse a previously created function, either to populate the current function fields or as a template to create a function.
To use a previously created function
  1. In the Function Builder window, click
    Import
    .
    The
    Saved Functions
    window opens.
    The
    Saved Functions
    window lists all functions that were previously created in the current ACD file. Columns list the function name, result type, and function type.
    TIP:
    If any functions are no longer used, click
    Delete
    to delete them.
  2. Select a saved function and click
    OK
    . The saved function populates the
    Function Builder
    window.
  3. Click
    OK
    to reuse the function or edit the fields to create a function.
    IMPORTANT:
    Function names must be unique within a library object. A warning displays when the function name matches the name of an existing function in the current library object. Rename the function to be unique.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal