Edit a function
A function is an argument that is not exposed to external access. The value of a function is generated by user-defined logic created in the
Library Designer
and by conditions that apply during instantiation. Edit a function when needed, such as to add branches to a conditional statement or update an expression.To edit a function
- In the decorator pane, click theFunctionstab, then either:
- Double-click the function.
- Right-click the function, then selectEdit.TheFunction Builderwindow opens.
- Edit the function.
- ClickOKto save the changes to the function.
Provide Feedback