Delete branches

A conditional function allows for multiple branches and nesting. The additional branches and nested conditions can be deleted if they are not needed.
To delete branches from a conditional statement
  1. Right-click an item in the conditional statement menu tree.
  2. Select
    Delete
    .
    TIP:
    The root IF or ELSE statements cannot be deleted.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal