Delete a function

Delete a function if it is no longer used.
TIP:
Use the
Show References
command to list references to the function before using the
Delete
command.
To delete a function
  1. Right-click the function, then select
    Delete
    . The
    Delete Objects
    window opens.
  2. To finish the deletion, click
    Yes
    .
    TIP:
    A warning window displays if the function is referenced.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal