Copy a function

A function can be copied from one library object to another library object.
To copy a function to a different library object
  1. In the decoration pane, click the
    Functions
    tab.
  2. Right-click the function, then select
    Copy
    .
  3. In the
    Library Objects
    pane, click the other library object.
  4. In the decoration pane, click the
    Functions
    tab.
  5. Right-click a group name, then select
    Paste
    .
    The function is added to the library object.
    TIP:
    If the library object does not contain all of the decorative elements referenced by the function, the Function Builder window opens with any statements that contain missing elements outlined in red.
    The function is pasted into the library object even if the missing elements are not resolved.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal