Track Logix content changes
Use
Library Designer
to track Logix content changes in Logix Designer
since the last time Library Designer was launched. When Logix contents have been changed in Logix Designer
, notifications in the form of an asterix (*) appear in Library Designer
next to the relative library content. The notifications will be cleared automatically when Library Designer
is closed and the tracking is updated.Tracking changes may take some time and will impact performance.
To track Logix content changes
- Add library objects in theSelected Objectscolumn to theLibrary Objectscolumn.
- On theLibrary Objectstoolbar, clickTools > Track Logix content changes. Notifications appear when Logix contents are changed inLogix Designer.TIP:If Logix contents are deleted inLogix Designer, the notification appears on the parent folder.
- ClickOK.
Provide Feedback