Show library object dependencies
If the
Add Dependencies
option is selected when adding the library object, all dependencies are automatically included in the object.Use the
Show or Hide Dependencies
setting to show or hide the dependent objects.Showing dependencies may take some time and will impact performance.
To show library object dependencies
- In theLibrary Objectspane, either:
- Right-click the library object, and then clickShow dependencies.
- Click the library object, and then on theLibrary Objectstoolbar, click theShow dependencies for all librariesbutton.TIP:SelectingShow dependencieswhen theLibrariesnode is selected will show all dependencies of all library objects in the tree.
- A confirmation message shows, indicating that showing all library object dependencies will affect performance. ClickOK.
Provide Feedback