Publish a library

Publish a library for it to be available for use by other applications. Library objects can be published to an existing
Library Object Manager
repository, a folder, or an ACM database.
To publish a library
  1. In the
    Library Objects
    pane, either:
    • Select the
      Libraries
      item to publish all libraries.
    • Press
      Shift
      and click adjacent library objects.
    • Press
      Ctrl
      and click multiple library objects.
    • Click a library object.
  2. Right-click the highlighted selection and then click
    Publish Library
    .
    The
    Library Destination
    window opens.
  3. Select one of the following destinations for the published library:
    • LOM Repository
      Select from the list of repositories configured in
      Library Object Manager
      .
    • Folder
      Type the path to a folder to publish the library or click the ellipsis (...) to browse for a folder.
    • Current ACM Database
      Automatically connects to the last ACM database instance used.
    • Another ACM Database
      Click the ellipsis (...) button to open the Connection Properties window and connect to a different ACM database.
  4. The
    Library Import Configuration
    window opens.
    • Enter a
      Revision Description
      for each library object listed.
    • The library attributes configured on the library property in the ACD file will be used as the primary values.
    • Once all of the required parameters are entered, click
      OK
      .
      TIP:
      If the
      OK
      button is disabled, a required parameter has not been specified.
  5. After the publication process completes, the
    Library Publication
    dialog box displays the
    Library Published
    message. Click
    OK
    to close the dialog box and return to
    Library Designer
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal