Parameters for a library object
Use the
Library Import Configuration
window to define the parameter settings for a library object that is being published from Library Designer
into a library repository.The
Library Import Configuration
window has these settings.Name | Type | Description |
|---|---|---|
01 Library Status | ||
Status | Dropdown menu | If the library is saved as Pending, this revision will be replaced next time changes are saved. If the library is saved as Published, a new revision will be created next time changes are saved. |
02 Revision History | ||
Revision Description | Text entry | The revision description of the library object. This is an optional setting. |
Reset History | Dropdown menu | Displays different options to keep the current revision history, remove previous revision histories, or clear all revision histories. This is a required setting. |
03 Library Details | ||
CatalogNumber | Text entry | The library object name, which appears together with the revision number in the library object listing when the library object is registered in ACM. This is entered manually. This is a required setting. |
Description | Text entry | The description of the library object. This is an optional setting. |
Family | Dropdown menu | The Family of the library object. This is a required setting. |
Solution | Dropdown menu | The Solution for the library object. This is a required setting. |
Library Type | Dropdown menu | The Library Type for the library object. This is a required setting. |
Category | Dropdown menu | The Category for the library object. This is a required setting. |
Content Type | Text | Displays the type of the object, Task, Program, or Routine. |
Owner | Text entry | The user or entity that originally published the library object. This is a required setting. |
Major Revision | Text entry (integer) | The major revision number for the library object. For a new library object, this defaults to 1. If you are updating an existing library a new value will be set based on existing library objects with the same CatalogNumber, unless the library status is Pending. |
Minor Revision | Text entry (integer) | The minor revision number for the library object. For a new library object, this defaults to 0. If you are updating an existing library a new value will be set based on existing library objects with the same CatalogNumber, unless the library status is Pending. |
04 Library Usage Rules | ||
Upstream Keys | Text entry | For module library objects: a rule that limits the upstream hardware components
that will be made accessible to the library object when it is added to an ACM
Project. The rule is entered manually as a logical expression. |
Downstream Keys | Text entry | For module library objects: a rule that limits the downstream hardware components
that will be made accessible to the library object when it is added to an ACM
Project. The rule is entered manually as a logical expression. |
Provide Feedback