Order programs in a library
When a library is of content type
Program
in Library Designer
, you can rearrange the order of the programs in that library as needed. Once you use the library in Application Code Manager
and publish the controller to an ACD file, the order of the programs you customized will display in Studio 5000 Logix Designer
.To order programs in a library of content type Program
- InLibrary Objects, expand the library of content typeProgram.
- Right-clickPrograms, and then selectOrder Programs.
- InOrder Programs, select a program, and then click theUporDownbutton to rearrange the programs.
- SelectOK.
- In theLibrary Designerwindow, selectApplyto save changes.
Provide Feedback