Module Wizard overview

How do I open the Module Wizard?
  • Add the module object to a library object of module type. The
    Module Wizard
    opens.
  • Assign to or create a library object of module type. The
    Assign to/Create New
    window opens, and then select
    OK
    . The
    Module Wizard
    opens.
  • Right-click a Module that has already been added to a library and select Decorate Library.
The
Module Wizard
generates default parameters and subobjects for the library object based on the controller code for the module. This decoration conforms to the standards of the
Studio 5000 Logix Designer
design process. Accept the defaults or edit them in the wizard.
  • The
    Library Designer
    automatically assigns the
    Module Type
    . This field cannot be edited.
  • The
    Library Designer
    displays the same structure of the
    I/O Configuration
    tree as it in
    Studio 5000 Logix Designer
    , which makes decorating non-rack modules or devices easier.
  • The
    Library Designer
    generates an initial set of parameters. The
    Parameter Name
    field cannot be edited. The
    Default Value
    field is editable by double-clicking in the field. For parameters with a data type of
    Integer
    , the
    Min
    and
    Max
    are editable by double-clicking in the field. The
    Apply
    checkbox determines whether the parameter is included in the library object. All boxes are checked by default.
  • The
    Library Designer
    generates an initial set of subobjects. For example, an analog input module opens in the wizard with Analog Input (AI) and Analog Output (AO) subobjects. The
    Channel Type
    field is not editable. Other fields are editable; double-click in the field to open it for editing. Parameter names appear enclosed in angle brackets. The
    Apply
    checkbox determines whether the SubObject will be included in the library object. All boxes are checked by default.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal