Include dependent objects
For object elements to be available to the application, they must be included in the library. The color of the object name in the
Library Objects
tree denotes whether the element is included in the library. The name of dependent objects included in the library is displayed using black text while the name of elements that are not included in the library are displayed using gray text. When objects that are not included in the library are selected in the Library Objects
tree the decorator pane is blank.To include dependent objects
- In theLibrary Objectspane, right-click the library object and then clickInclude in this library.TIP:SelectShift+Clickto select multiple sequential library objects to include.SelectCtrl+Clickto select multiple individual objects to include.
- The decorator pane updates to show the attributes and parameters of the object and the library.If multiple objects are being included, the decorator pane flashes several times and displays aNamevalue of**Multiple Objects**.The object name in theLibrary Objectstree changes from gray to black indicating that it has been included.
Provide Feedback