Import library object parameters

Import parameters to an
Excel
spreadsheet to transfer them from another system or to restore a backup copy of library object parameters. The import can include multiple library objects or individual library objects. The library objects must exist to import parameters. This process does not create library objects.
To import library object parameters
  1. In the
    Library Objects
    pane, either:
    • Click the
      Libraries
      node.
    • Click an individual library.
  2. On the
    Library Objects
    toolbar, click
    Tools > Import Parameters
    .
  3. Browse to and select an import file, then select
    Open
    .
  4. A green progress bar appears at the bottom of the
    Library Designer
    window.
    Once the import process has completed, the imported parameters are displayed in the decorations panel of the library object on the
    Parameters
    tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal