Hide library object dependencies

If the
Add Dependencies
option is selected when adding the library object, all dependencies are automatically included in the object.
Use
Show dependencies
or
Hide dependencies
to show or hide the dependent objects.
Hiding dependencies may take some time and will impact performance.
To hide library object dependencies
  1. In the
    Library Objects
    pane, either:
    • Right-click the library object, and then click
      Hide dependencies
      .
    • Click the library object, and then on the
      Library Objects
      toolbar, click the
      Hide dependencies for all libraries
      button.
      TIP:
      Selecting
      Hide dependencies
      when the
      Libraries
      node is selected will hide the dependencies of all library objects in the tree.
  2. A confirmation message shows, indicating that hiding all library object dependencies will affect performance. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal