Export library object parameters
Export parameters to a
Microsoft®
Excel®
spreadsheet to transfer them to another system or to make a
backup copy of library objects. All of the libraries can be exported in one process or
individual libraries can be exported.To export library object parameters
- In theLibrary Objectspane, either:
- Click theLibrariesnode.
- Click an individual library.
- On theLibrary Objectstoolbar, clickTools > Export Parameters.
- A green progress bar appears at the bottom of theLibrary Designerwindow.Once the export process has completed, anExcelspreadsheet is opened containing the exported parameters.
- To retain the parameters file, inExcelclickFile >Save.
Provide Feedback