Create an empty parameters file

Use an empty library objects parameters file to enter data for library object parameters manually. The empty parameters file can be scoped to all libraries or to a single library.
To create an empty library object parameters file
  1. In the
    Library Objects
    pane, either:
    • Click the
      Libraries
      node.
    • Click an individual library.
  2. On the
    Library Objects
    toolbar, click
    Tools > Export Parameters
    .
  3. A green progress bar appears at the bottom of the
    Library Designer
    window.
    • If the
      Libraries
      node was selected, an
      Excel
      spreadsheet is opened containing tabs for each library object.
    • If an individual library was selected, and
      Excel
      spreadsheet is opened containing a single tab for the selected library object.
  4. To retain the parameters file, in
    Excel
    click
    File > Save
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal