Copy and paste a library

In
Library Designer
, before you update an existing library object, you can copy and paste a whole library to create a backup or create a variant of the original library.
To copy and paste a library
  1. In
    Library Objects
    , expand
    Custom Properties
    , and then expand
    Libraries
    .
  2. Right-click the library object that you want to copy, and then select
    Copy
    .
  3. Right-click
    Libraries
    , and then select
    Paste
    .
  4. In the
    Library Designer
    window, select
    Apply
    to save changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal