Assign to/Create New window
How do I open the Assign to/Create New window?
- On theSelected Objectstoolbar, clickAdd selected object to a Library.
- On theLibrary Objectstoolbar, clickCreate a New Library.
- Drag or paste items fromSelected Objectsto the topLibrariesnode inLibrary Objects.
The
Assign to/Create New
window is used to populate library objects. It can be used to bring items from the ACD file into existing library objects that can be edited using Library Designer
or to create library objects that contain the item from the ACD file. Additionally, when opened from the Library Object
pane it can be used to create new empty, library objects.When an existing library is being used, only
Select Library
is active; all Library Attributes
settings in this window are read-only.When creating a library object, all of the settings except for
Revision
become active.This window opens when you click the
Add selected object to a Library
button.The
Assign to/Create New
window has these settings.Name | Type | Description |
|---|---|---|
Select Library | Dropdown menu | Choose which of the existing library objects an item should be assigned to. Visible when using items originating from an ACD file or after clicking Add selected object to a Library on the Select Objects toolbar. |
Create New | Checkbox | Select to create a library object and assign the item to it. Visible when using items originating from an ACD file or after clicking the Add selected object to a Library button on the Select Objects toolbar. |
Catalog Number | Text entry | The library object name, which appears when the library object is registered in the Application Code Manager application. |
Revision | Auto | Dimmed field, displays the system-generated version of the library object. |
Description | Text entry | The description of the library object. |
Library Type | Dropdown menu | Selects the library type and identifies the library object as a module. A module registers as hardware rather than software in the Application Code Manager application. |
Content Type | Dropdown menu | Selects the object type, Task , Program , or Routine . |
Base Library | Dropdown menu | Selects an existing library object in the library object hierarchy as a base library. When a base library is selected, the current library object inherits substitutions from the base library, and the Expression Builder accesses all custom properties of the base library when used in the current library object. When None is selected, the current library object does not inherit custom properties. |
Solution | Dropdown menu | This list is empty if no solution has been set in another library in the same ACD or if the Settings file is also empty. |
Family | Dropdown menu | Selects a family from the list. |
Category | Dropdown menu | Selects a category from the list. |
Instantiation: Name | Text entry | Sets the name for each instantiation of the library object. To use a calculated value for this field, click the ellipsis (...) button next to the field to open the Expression Builder . |
Instantiation: Description | Text entry | Sets the default description for each instantiation of the library object. To use a calculated value for this field, click the ellipsis (...) button next to the field to open the Expression Builder . |
Substitutions: Name | Text entry | Sets the default substitution for a text string in the library object name when the library object is instantiated. This string can be the complete name or a substring within the name. The substitution extends to the names of all elements within the library object. By default, the Library Object Manager application assigns the predefined parameter {ObjectName} as the substitution for the entered string. |
Substitutions: Description | Text entry | Sets the default substitution for a text string in the library object description when the library object is instantiated. This string can be the complete description or a substring within the description. The substitution extends to the descriptions of all elements within the library object. By default, the Library Object Manager application assigns the predefined parameter {ObjectDescription} as the substitution for the entered string. |
Provide Feedback