Advanced connection properties
The
Advanced Properties
dialog box provides a means of changing how the connection between the Library Designer
and the ACM database passes information. This table describes the settings in the
Advanced Properties
dialog box. The dialog box is divided into functional areas.
TIP:
Applying the recommended settings will improve ACM performance especially for network connections.
Area | Setting | Possible Values | Description |
|---|---|---|---|
Advanced | MultipleActiveResultSets | True False (default) | When True, multiple result sets can be returned and read from one connection. |
Network Library | blank (required if local) Named Pipes (DBNMPNTW) Shared Memory (DBMSLPCN) TCP/IP (DBMSSOCN) (recommended if networked) VIA (DBMSGNET) | The network library used to establish a connection to an instance of SQL Server . Do not use when the SQL Server is resident on the local host computer, value should be blank. | |
Packet Size | 8000 (recommended) | Size in bytes of the network packets used to communicate with an instance of SQL Server . PacketSize may be a value in the range of 512 bytes
and 32,767 bytes. | |
Transaction Binding | Implicit Unbind (default) Explicit Unbind | Indicates the binding behavior of connection to the System.Transactions namespace.When set to Implicit Unbind , the connection detaches from the transaction when it ends, switching back to autocommit mode.When set to Explicit Unbind the connection remains attached to the transaction until the transaction is closed. The connection will fail if the associated transaction is not active or does not match the current transaction. | |
Type System Version | Latest (default) SQL Server 2012SQL Server 2008SQL Server 2005 | Indicates which server type system the provider will expose through the DataReader. | |
Connection Resiliency | ConnectRetryCount | 2 (recommended) | Number of attempts to restore a connection. The number of reconnections attempted after identifying that there was a connection failure. This must be an integer between 0 and 255. Set to 0 to disable reconnecting on idle connection failures. |
ConnectRetryInterval | 5 (recommended) | Delay between attempts to restore connection. The amount of time (in seconds) between each reconnection attempt after identifying that there was a connection failure. This must be an integer between 1 and 60. | |
Context | Application Name | .Net SqlClient Data Provider | The name of the application. |
Workstation ID | The name of the workstation connecting to SQL Server . | ||
Initialization | ApplicationIntent | ReadWrite (default) ReadOnly | Declares the application workload type when connecting to a server. |
Asynchronous Processing | True False (default) | When true, enables usage of the Asynchronous functionality in the .NET Framework Data Provider. | |
Connect Timeout | 30 (recommended) | The length of time in seconds to wait for a connection to the server before ending the attempt and generating an error. A value of 0 indicates no limit, and should be avoided in a ConnectionString because an attempt to connect waits indefinitely. | |
Current Language | The SQL Server Language record name. | ||
Pooling | Enlist | True (default) False | When True , sessions in a Component Services environment should automatically be enlisted in a global transaction where required. |
Load Balance Timeout | 30 (default) | The minimum amount of time (in seconds) for this connection to live in the pool before being destroyed. When a connection is returned to the pool, its creation time is compared with the current time, and the connection is destroyed if that time span (in seconds) exceeds the value specified by Load Balance Timeout . A value of zero (0) causes pooled connections to have the maximum connection timeout. | |
Max Pool Size | 1000 (recommended) | The maximum number of connections allowed in the pool. Valid values are greater than or equal to 1. Values that are less than Min Pool Size generate an error. | |
Min Pool Size | 1 (default) | The minimum number of connections allowed in the pool. Valid values are greater than or equal to 0. Zero (0) in this field means that no minimum connections are initially opened. Values that are greater than Max Pool Size generate an error. | |
PoolBlockingPeriod | Auto AlwaysBlock NeverBlock (recommended) | Defines the blocking period behavior for a connection pool. When connection pooling is enabled and a timeout error or other sign-in error occurs, an exception will be thrown and subsequent connection attempts will fail for the next five seconds, the "blocking period". If the application attempts to connect within the blocking period, the first exception will be thrown again. Subsequent failures after a blocking period ends will result in a new blocking period that is twice as long as the previous blocking period, up to a maximum of one minute. | |
Pooling | True (recommended) False | When True , the connection object is drawn from the appropriate pool, or if necessary, is created and added to the appropriate pool.Any newly created connection is added to the pool when closed by the application. In the next attempt to open the same connection, that connection will be drawn from the pool. Connections are considered the same if they have the same connection string. Different connections have different connection strings. | |
Replication | Replication | False (default) True | Used by SQL Server in replication.Set to True if replication is supported using the connection. |
Security | Authentication | NotSpecified (default) SqlPassword ActiveDirectoryPassword ActiveDirectoryIntegrated | Specifies the method of authenticating with SQL Server . |
Column Encryption Setting | Enabled Disabled (default) | Default column encryption setting for all the commands on the connection. | |
Encrypt | True False (default) | When True, SQL Server uses SSL encryption for all data sent between the client and server if the server has a certificate installed. | |
Integrated Security | True False (default) | Whether the connection is to be a secure connection or not. When False , User ID and Password are specified in the connection. When True , the current Windows account credentials are used for authentication. | |
Password | ******* | Indicates the password to be used when connecting to the data source. | |
Persist Security Info | True False (default) | When False , security-sensitive information, such as the password, is not returned as part of the connection if the connection is open or has ever been in an open state. | |
TrustServerCertificate | True (recommended) False | When True (and Encrypt is set to True ), SQL Server uses SSL encryption for all data sent between the client and server without validating the server certificate. If TrustServerCertificate is set to True and Encrypt is set to False , the channel is not encrypted. | |
User ID | sa | Indicates the user ID to be used when connecting to the data source. | |
Source | AttachDbFilename | The name of the primary file, including the full path name, of an attachable database. | |
Context Connection | True False (default) | When True , indicates that the connection should be from the SQL Server context. Available only when running in the SQL Server process. | |
Data Source | localhost\SQLACM (default) | Indicates the name of the data source to connect to. | |
Failover Partner | The name or network address of the instance of SQL Server that acts as a failover partner. | ||
Initial Catalog | Initial Database Name | The name of the initial catalog or database in the data source. | |
MultiSubnetFailover | True False (default) | If your application is connecting to a high availability, disaster recovery (AlwaysOn) availability group (AG) on different subnets, setting this value to True configures SqlConnection to provide faster detection of and connection to the (currently) active server. | |
TransparentNetworkIPResolution | True (default) False | If your application connects to different networks, setting this value to True configures SqlConnection to provide transparent connection resolution to the currently active server, independently of the network IP topology.When set to True , the application is required to retrieve all IP addresses for a particular DNS entry and attempt to connect with the first one in the list. If the connection is not established within 0.5 seconds, the application will try to connect to all other IP addresses in parallel. When the first IP address answers, the application will establish the connection with the respondent IP address.If MultiSubnetFailover is set to True , this setting is ignored.If Failover Partner is specified, this setting is ignored.The default setting is False if Authentication is set to either Active Directory Password or Active Directory Integrated , otherwise the default setting is True . | |
User Instance | True False (default) | Indicates whether the connection will be redirected to connect to an instance of SQL Server running under the user's account. |
Provide Feedback