Add a module to a library object
Module objects are listed in the
Selected Object
tree view under the I/O Configuration
node. These objects may be added to a library object. The Library Designer
recognizes the selected object as a module and opens the Module Wizard
.To add a module to a library object
- Select a module object in theSelected Objecttree view.
- Add the module object to a library object. The Module is added to the library object and theModule Wizardopens.
- (optional) Double-click to edit theDefault Valuein the initial set of parameters. If the parameter is anIntegerdata type, theMinandMaxvalues are also editable.TIP:TheParameter Nameis not editable.
- (optional) Select Apply to include the parameter in the library object.
- (optional) Double-click to edit the initial set of subobjects. Parameter names appear enclosed in angle brackets.TIP:TheChannel Typeis not editable.
- (optional) Select Apply to include the subobjects in the library object.
Provide Feedback