Sequence Detail Control command controls
Use these commands to control an
Equipment Sequence
using the Sequence Detail Control. The availability of some commands depends on the selected Equipment Sequence
owner, state, mode, and failure status. Select More
to display all the commands on the toolbar.These commands are always displayed:
- Take/Release ownership
- Set ID
- Start
- Hold
- Restart
- Stop
- Abort
- Reset
- More/Less
These commands are available after selecting the
More
button and can be hidden by selecting the Less
button:- Initialize parameters
- Clear Failures
- Pause/Cancel Pause
- Auto Pause/Cancel Auto Pause
- Resume
- Enter/Exit Manual
- Step change
- Force transition
Icon | Command | Description |
![]() | Take Ownership | Take ownership of the Equipment Sequence . Taking ownership means that this application now has the right to command this Equipment Sequence ; other internal sequencers, external sequencers, and operators are not allowed to command this sequence. |
![]() | Release Ownership | Release ownership of the Equipment Sequence . Releasing ownership means that internal sequencers, external sequencers, and operators with attachments are allowed to command this sequence. |
![]() | Set ID | Opens the Set Sequence ID dialog box where you can assign an identifier of up to 82 characters to the Equipment Sequence . This command is enabled only when an Equipment Sequence is idle. |
Initialize Parameters | Reinitialize all sequencing parameter and step tag value fields with their configured Initial Value. | |
Step Change | Make the next step of the Equipment Sequence active and able to be commanded. | |
Start | Start execution of the Equipment Sequence . | |
Hold | Halt all connected phases for the Equipment Sequence and stop evaluating transitions until the Equipment Phase runs its Hold routine. | |
Restart | Resume execution of the Equipment Sequence from the HELD state. | |
Stop | Stop all connected phases and active transitions for the Equipment Sequence . | |
Abort | Abort all connected phases and active transitions for the Equipment Sequence . | |
Reset | Reset any remaining active phases for the Equipment Sequence . | |
Clear Failures | Clear the failure flags on the Equipment Sequence . | |
![]() | Pause | Pause execution of the Equipment Sequence . When the active transition evaluates TRUE, it does not transition to the FIRING state until you select Resume . When paused, select to cancel pause. |
![]() | Auto-Pause | Automatically pause the Equipment Sequence as transitions evaluate TRUE. When you select Resume , the next transitions fires, but the Equipment Sequence pauses again after each transition evaluates TRUE. When auto-pause is enabled, select to cancel auto-pause. |
Resume | Continue execution of the Equipment Sequence when the substate is Paused.. | |
Enter Manual | Put the Equipment Sequence in Manual mode, in which the sequencing engine does not automatically fire transitions, and an operator commands the Equipment Sequence step by step. On the toolbar, only the Release Ownership , Pause , Auto-Pause , and Automatic commands are enabled. | |
Exit Manual | Put the Equipment Sequence in Automatic mode, which allows the sequencing engine to automatically fire transitions and execute the Equipment Sequence . |
Provide Feedback