Description: Sequencing Parameters Control

The
Sequence Parameters Control
displays a table of all sequencing parameters and step tags of a specified
Equipment Sequence
, and allows the operator to command a selected sequencing parameter or step tag. To refine the display, configure the table to filter the displayed information.
Sequence Parameters Control validates the value so it is within the configured Min and Max range.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal