Tips for using array tags
To create an array tag, specify how many elements to use, beginning with the first element at the tag’s address.
Use these tag data types for array tags. Use this table to determine how many data elements to address to provide the number of bits you need.
Data Type | Number of bits per element |
|---|---|
Character | 8 |
Byte | 8 |
Short Integer | 16 |
Word | 16 |
Integer | 32 |
Double Word | 32 |
For example, if you want to monitor 128 bit positions for an alarm trigger, and you are using the Integer data type, you would append the modifier L4 to the tag name (because 4 x 32 = 128).
You cannot use HMI tags (digital or string tags) for array tags. You must use a direct reference (data server tags) for array tags.
Equivalent data types
Different processors and OPC servers use different terminology for tag data types. This section provides information about equivalent data types that you can use for array tags, with the associated number of bits for each.
Analog HMI tags created in FactoryTalk View
You can view a tag’s data type in the Tag Browser.
Data type | Number of bits |
|---|---|
Byte | 8 |
Unsigned Integer | 16 |
Integer | 16 |
3-Digit BCD | 16 |
4-Digit BCD | 16 |
Long Integer | 32 |
PLC and SLC tags
When creating array tags, you can use PLC and SLC tags with this data type:
Data type | Number of bits |
|---|---|
Short Integer | 16 |
Data server tags with the Short Integer data type are shown in the
Tag Browser
with the Item Canonical Data Type of Integer.Studio 5000 tags
When creating array tags, you can use Studio 5000 tags with these data types:
Table Heading | Table Heading |
|---|---|
SINT | 8 |
INT | 16 |
DINT | 32 |
Data server tags with the data types described in the table are shown in the
Tag Browser
with the Item Canonical Data Types of Character, Short Integer, and Long Integer, respectively.Provide Feedback