Causes of runtime errors for macros

At runtime, the application logs errors and warnings about macros to diagnostics under these circumstances:
  • problems reading the macro file or the expression
  • problems writing to the tag
  • problems communicating within the project or with the data source
The application also sends information messages to diagnostics when an expression in a macro is read successfully, and when a value is written to a tag successfully.
TIP:
Because macros are not necessarily run in the order in which they are listed, do not rely on the order of execution to control your process.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal