Replace tag placeholders in test display mode

The
Test Display
dialog box appears when testing a display if one or more tag placeholders are defined in the display. You can specify a parameter file or list to replace them with the actual tag names. You can also click
Cancel
to quit the display testing and go back to the Edit mode.
TIP:
# followed by a number is reserved for tag placeholders. It is not recommended to use this format in other cases, such as static text. If you must use # followed by a number in static text, add a space or _ between # and the number. For example, enter
#_3
or
# 3
.
Parameter File
Select this option if the parameter values will be provided by a parameter file.
Click the browse button and select a file in the
Component Browser
. The parameter file assigns tags to tag placeholders in the display when the display runs.
Parameter List
Select this option if the parameter values will be provided by a parameter list.
All tag placeholders in the display are listed. Enter a tag name or value for the placeholder. You can also click the browse button to select a tag.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal