Select import type

To select the import type
  • From the list, select the type of application file that you want to import.
    TIP:
    If you are creating a new application from an existing
    FactoryTalk View ME
    project (*.med), use a name for the new application that is different from the existing project name.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal