Create a FactoryTalk View ME Station project

You can use the
New Project
dialog box to create a
FactoryTalk View ME Station
project.
To create a
FactoryTalk View ME Station
project
  1. Select
    Station
    under the
    View ME
    category.
  2. Click
    Next
    .
  3. (optional) Type a description for the project.
    The description is limited to 255 bytes. Standard ASCII characters consume 1 byte per character, allowing for 255 characters. Note that some characters (for instance, those used for Asian languages), take up to three bytes to represent one character, resulting in less than 255 characters maximum.
  4. Select a language for the project.
  5. Define
    Resolution
    for the project. For details, see Specify project settings (General tab) in
    FactoryTalk View ME
    Help.
  6. Click
    Finish
    to close the
    New Project
    wizard and open the project in
    FactoryTalk View Studio
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal