Create a MobileView or PanelView Plus project
You can use the
New Project
dialog box to create a MobileView
or PanelView Plus
project.To create a
MobileView
or PanelView Plus
project- Select one of the following terminals under theView MEcategory, on which you run the project:
- MobileView
- PanelView Plus 6
- PanelView Plus 6 Compact
- PanelView Plus 7 Performance
- PanelView Plus 7 Standard
- Select a terminal size under the selected terminal.
- ClickNext.
- (optional) Type a description for the project.The description is limited to 255 bytes. Standard ASCII characters consume 1 byte per character, allowing for 255 characters. Note that some characters (for instance, those used for Asian languages), take up to three bytes to represent one character, resulting in less than 255 characters maximum.
- Select a language for the project.
- ClickFinishto close theNew Projectwizard and open the project inFactoryTalk View Studio.
Provide Feedback