Router factory settings and identification

The following table shows the factory settings of router interfaces:
Interface
IP Address
Mask
LAN
192.168.0.1
255.255.255.0
WAN
DHCP
The router settings configuration is protected with user/password credentials.
  • The default (not changeable) user is
    admin
    .
  • The default password (configurable) is
    admin
    .
Factory settings information is located on the router side, together with the MAC addresses of both LAN and WAN network interfaces.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.