Ingress Egress Object

FactoryTalk Policy Manager
supports the Ingress Egress Object for
ODVA™
devices.

Overview

The Ingress Egress Object is a set of rules that govern which network nodes can communicate to the device and through the device.
Ingress rules
Determine which nodes can communicate with the device.
Egress rules
Determine how the device can communicate with other nodes.

Specifications

FactoryTalk Policy Manager
supports both the
ODVA
Ingress Egress Object and
Rockwell Automation
Ingress Egress Object. The
ODVA
Ingress Egress Object takes precedence over the
Rockwell Automation
Ingress Egress Object.
Ingress Egress Object resolution matrix
Ingress Egress Objects on device
Ingress Egress Object
ODVA
Ingress Egress Object
ODVA
Ingress Egress Object
ODVA
Ingress Egress Object and
Rockwell Automation
Ingress Egress Object
ODVA
Ingress Egress Object
Rockwell Automation
Ingress Egress Object
Rockwell Automation
Ingress Egress Object
No Ingress Egress Object
No Ingress Egress Object
For more information about the
ODVA
Ingress Egress Object, refer to the
ODVA
documentation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal