Application notes
These application notes apply to
FactoryTalk Optix
version 1.3.x.Threat mitigation
- Do not lose the USB Key with exportedFactoryTalk Optix Application. The USB key contains inspectable fields, credentials, certificates, and hashed passwords.
- Protect physical access toRockwell Automationmanufactured devices.
- Do not leave connected devices unattended. Protect physical access to the device and protect logs from device web interface, connected diagnostic session, and file system access via remote assistance tool.
- Prevent unauthorized physical access to the device. Protect physical access to the device and improve security level of application files generated by custom logics.
- Protect physical access to logged-in user sessions. Prevent the theft ofFactoryTalk Hubrefresh token file by locking the session if unattended.
- Protect physical access to logged-in user sessions. Prevent the removal ofFactoryTalk Hubrefresh token file by locking the session if unattended.
- Protect physical access to logged-in user sessions. Prevent attacks while logging in to GitHub.
Feature preview
Features labeled as preview should not be used in a production environment. Feature preview includes:
- RA EtherNet/IP communication driver in the FactoryTalk Optix Studio web editor and Emulator
- Connected IDE mode
- File sign and verify library object
- Model analysis providing information model graphs
- Micro Controller Driver. Connect Micro800™ and MicroLogix™1400 controllers through Ethernet or Serial.
- Smart Objects / Edge Apps
- Direct Drives Connectivity
- RAEthernet IP tag importer added extended properties to the imported tags Description, Engineering Unit, Min, and Max, as well as State0/State1 for Boolean tags. These extended properties display values from a controller on the HMI device.
Provide Feedback