Create a list box

Create a list box that displays data from the DataStore.
  1. Create a list box:
    1. In
      Project view
      , right-click
      MainWindow (type)
      and select
      New
      Data controls
      List box
      .
    2. Hover-over the list box, select
      Edit
      , and enter
      RandomDataListBox
      .
  2. Configure the list box:
    For more information about dynamic links, see Create dynamic links.
    1. In
      Properties
      , create a dynamic link between
      Model
      and
      ProjectName
      DataStores
      RandomStringsDataStore
      .
    2. Create a complex dynamic link between
      Query
      and
      Text
      of
      DataFilterTextBox
      by using a string formatter.
      Format
      SELECT Column1 FROM Table1 WHERE Column1 LIKE '%{0}%'
      {0} DynamicLink
      ProjectName
      UI
      MainWindow (type)
      DataFilterTextBox
      Text
      For more information about dynamic links, see Create dynamic links.
    3. Create a dynamic link between
      Display value path
      and
      {Aliases}
      {Item}
      PointedNode
      Column1
      .
      TIP: You may need to enter
      Column1
      manually.
      For more information about dynamic links, see Create dynamic links.
    4. Create a dynamic link between
      Order by
      and
      {Aliases}
      {Item}
      PointedNode
      Column1
      .
      TIP: You may need to enter
      Column1
      manually.
      For more information about dynamic links, see Create dynamic links.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.