CODESYS Tag

BrowseName
CODESYSTag
SuperType
Tag(Tag)

Properties

Name
BrowseName
DataType
Description
Symbol name
SymbolName
Tag name.
Maximum length
MaximumLength
(string data only) Maximum number of characters in the string.
Encoding
Encoding
Decode of memory location contents mode.
Start array index
StartArrayIndex
Array update mode
ArrayUpdateMode
(Inherited from Tag)
Original data type
OriginalDataType
(Inherited from Tag)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal