Events
Events are circumstances that occur at runtime. When the event occurs, it performs an action or method.
For example, a button release may be the event that performs the method of increasing a value in a variable. Events can perform methods either when a user takes an action or a specified circumstance occurs in the
FactoryTalk Optix Studio
application. in Project view
indicates that an item is an event. Provide Feedback