Property panel

When you select an object, the
Property
panel displays a set of properties.
Properties panel
Property panel options
Button
Function
Organize the properties in groups.
Sort the properties in alphabetical order.
Add a property to the node.
Remove a property or reset a property to its default value.
Open the object in the dedicated editor. This button is valid only for some object types.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.