Selection changed

BrowseName
UserSelectionChanged
SuperType
BaseEventType(BaseEventType)

Properties

Name
BrowseName
DataType
Description
Selected item
SelectedItem
Element selected when the object is initialized at runtime (if empty, it is initialized without selections). After initialization, this property displays the node corresponding to the selected element (access to the property is both read and write when the data are obtained from project nodes, read-only when obtained from a database).
Selected value
SelectedValue
Value of the property set in Path of the value selected when an element is selected at runtime.
EventId
(Inherited from BaseEventType)
EventType
(Inherited from BaseEventType)
SourceNode
(Inherited from BaseEventType)
SourceName
(Inherited from BaseEventType)
Time
(Inherited from BaseEventType)
ReceiveTime
(Inherited from BaseEventType)
LocalTime
(Inherited from BaseEventType)
Message
(Inherited from BaseEventType)
Severity
(Inherited from BaseEventType)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.