TwinCAT driver

Driver to communicate with the controller via the TwinCAT protocol.
BrowseName
TwinCATDriver
SuperType
Communication driver(CommunicationDriver)

Properties

Name
BrowseName
DataType
Description
Runtime import
AllowRuntimeTagImport
Enables the importation of the tags by the FactoryTalk Optix Application at runtime directly from the controller.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.